The running status of the CIMPLICITY project.
![]() |
RunningStatusGetResponse
The running status of the CIMPLICITY project.
|
Name | Description | Data Type |
---|---|---|
IsProjectRunning | represents the CIMPLICITY project is in run mode. | boolean |
IsPrimaryRunning | represents the CIMPLICITY Primary node is in run mode. | boolean |
IsSecondaryRunning | represents the CIMPLICITY Secondary node is in run mode. | boolean |
IsStartAtBoot | indicates if the project is configured to start at boot. | boolean |